A fruitful development partnership as well as trusting and reliable relationship such as the one that has existed between Canadian machine manufacturer Husky Injection Molding Systems and control system supplier Beckhoff for roughly 20 years now is a rarity these days. Husky recently underscored this by honoring Beckhoff with its EMEA Supplier Award at the K 2019 trade show held in Düsseldorf, Germany, in October.
When Husky chose Beckhoff as its control systems supplier in 1999, the renowned company was ready to step off the beaten path and work with a pioneer in the area of PC-based control technology. Beckhoff was still a relatively young and small company at the time, so Husky’s decision was not without risk. That the company decided to move forward with Beckhoff may have been based in part on individual rapport, but most of all on Husky's trust in the trailblazing potential of the PC-based control philosophy of Hans Beckhoff. The openness of the Industrial PC platform, which was based on Windows standards, and the clear separation between software and hardware opened up a new world of competitive benefits for Husky. PC-based control replaced Husky’s legacy control concept, which was based on a multitude of dedicated controllers and PLC hardware, with a single Industrial PC and TwinCAT as an integrated software platform.
During the development phase, it quickly became apparent that Beckhoff, with a strong innovative spirit, was the perfect match for Husky as the technology leader in high-performance injection molding machines. Husky's technical challenges subsequently led to technological improvements and the development of new Beckhoff products. A prime example of the close cooperation between Husky and Beckhoff are advanced temperature sensor modules, which can be mounted directly on the injection molding machine without any special cables.
After a successful trial phase, Husky went into series production with Beckhoff control systems and declared them the standard for its entire machine portfolio. In 20 years of continuous cooperation, various generations of PC-based control systems have been installed in Husky machines as a result. Husky was also one of the first companies to rely on the fast EtherCAT standard introduced to the market by Beckhoff in 2003. With EtherCAT, Husky’s machines not only became faster, but also more accurate, which in turn increased their performance and quality while making them more resource-efficient. The technical and economic success of both companies went hand in hand with these developments.
Beckhoff considers itself a technology-driven company. At the same time, the innovations that have made Beckhoff a global player in the automation industry were developed through the close cooperation with customers and a deep understanding of the challenges they face. In Beckhoff, Husky has found a supplier with great flexibility and a global distribution network that ensures quick response times, service and support – even in the field. As an owner-managed company, Beckhoff also stands for dependable cooperation without sudden strategy changes, for continuity in support from long-term contact persons, and for quick decision-making infrastructures when solving technical challenges.
Industries
![Mr. Mohamed Mewafy](/media/pictures/contact/kontakt-personen/mohamed-mewafy.jpg)
Mr. Mohamed Mewafy
11/6 Said Zakaria Street
Al Sefarat District, Cairo 11471
Egypt