解除固定固定关闭

中国区总部
毕孚自动化设备贸易(上海)有限公司

市北智汇园4号楼
静安区汶水路 299 弄 9-10 号
上海, 200072, 中国

+86 21 6631 2666
info@beckhoff.com.cn
www.beckhoff.com.cn/zh-cn/

Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
    • Chapters
    • descriptions off, selected
    • subtitles off, selected

      2024年10月10日

      Vision 2024: Beckhoff Trade Show TV

      At Vision 2024, Beckhoff presented a complete ecosystem for industrial AI applications with a clear focus on executing AI models directly on the industrial controller. Find out more about products and use cases from our colleague Michael Busch, Product manager for TwinCAT Vision, in our Trade Show TV.

      更多关于此视频的信息

      TwinCAT Vision

      TwinCAT Vision

      TwinCAT Vision 集成式图像处理解决方案进一步完善了 TwinCAT 软件产品系列,适用于工业 4.0、质量优化及跟踪与追踪等应用。

      机器视觉

      机器视觉

      倍福拥有丰富的机器视觉硬件产品系列,可一站式提供完整的系统解决方案。

      机器学习 — 适用于所有自动化领域

      机器学习 — 适用于所有自动化领域

      倍福的机器学习(ML)解决方案能够无缝集成到 TwinCAT 3 中。

      TF7800 | TwinCAT 3 Vision Machine Learning

      TF7800 | TwinCAT 3 Vision Machine Learning

      TwinCAT 3 Vision Machine Learning provides an integrated machine learning (ML) solution for vision-specific use cases. Both the training and the implementation of the machine learning models take place in real time, and they even help machines to learn sophisticated data analyses automatically. This can be used to replace complex, manually created program constructs.

      TF7810 | TwinCAT 3 Vision Neural Network

      TF7810 | TwinCAT 3 Vision Neural Network

      TwinCAT 3 Vision Neural Network provides an integrated machine learning (ML) solution for vision-specific use cases. The implementation of the machine learning models takes place in real time. With the help of these models, complex data analyses can be learned automatically. This means that complex, manually created program constructs can be replaced.

      TE3850 | TwinCAT 3 Machine Learning Creator

      TE3850 | TwinCAT 3 Machine Learning Creator

      The TwinCAT 3 Machine Learning Creator automatically creates AI models based on data sets. These AI models can be optimized in terms of their accuracy and latency to ensure they run efficiently on Beckhoff Industrial PCs with TwinCAT products. The generated models can also still be used as standardized ONNX models beyond the Beckhoff product range. For use with TwinCAT products, a PLCopen XML with IEC 61131-3 code is created in addition to the ONNX file, which describes the complete AI pipeline and can be imported seamlessly into TwinCAT.

      TF3800 | TwinCAT 3 Machine Learning Inference Engine

      TF3800 | TwinCAT 3 Machine Learning Inference Engine

      The TF3800 TwinCAT 3 Function is a high-performance execution module (inference engine) for trained, conventional machine learning algorithms.

      TF3810 | TwinCAT 3 Neural Network Inference Engine

      TF3810 | TwinCAT 3 Neural Network Inference Engine

      The TF3810 TwinCAT 3 Function is a high-performance execution module (inference engine) for trained neural networks.

      TF3820 | TwinCAT 3 Machine Learning Server

      TF3820 | TwinCAT 3 Machine Learning Server

      The TF3820 TwinCAT 3 Machine Learning Server is a high-performance service for executing trained AI models with the option of using hardware accelerators.

      TF3830 | TwinCAT 3 Machine Learning Server Client

      TF3830 | TwinCAT 3 Machine Learning Server Client

      The TwinCAT 3 Machine Learning Server includes a connection to a local client as standard (local TwinCAT runtime). If (possibly further) TwinCAT runtimes need remote access to a TwinCAT 3 Machine Learning Server, these runtimes must each be equipped with a license for the TF3830 TwinCAT 3 Machine Learning Client.

      C6043 | Ultra-compact Industrial PC with NVIDIA® GPU

      C6043 | Ultra-compact Industrial PC with NVIDIA® GPU

      The C6043 extends the series of ultra-compact industrial PCs to include a high-performance device with a built-in slot for powerful graphics cards. With the latest Intel® Core™ processors and highly parallelizing NVIDIA® graphics processors, the PC becomes the perfect central control unit for ultra-sophisticated applications. These include applications with high demands on 3D graphics or deeply integrated Vision and AI program blocks with minimal cycle times. The Beckhoff TwinCAT 3 control software is capable of mapping this as a fully integrated solution – without any additional software or interfaces. With the additional freely assignable PCIe compact module slot, the C6043 can be flexibly expanded with supplementary functions.