我们的搭载 Arm® Cortex®-A53 处理器的 CX82xx 和 CX9240 系列嵌入式控制器现已上市,并且也支持 Linux® 操作系统。欢迎观看本期视频,了解更多关于搭载 Arm® Cortex® 处理器的未来设备的性能数据以及规划信息。
更多关于此视频的信息

CX8210 | Embedded PC with Arm® Cortex®-A53 and EtherCAT slave
The CX8210 Embedded PC is a control with an EtherCAT slave interface. It features an Arm® Cortex®-A53 dual-core processor with 1.2 GHz. The basic configuration of the CX8200 includes a 1 Gbit Ethernet interface, a USB 3.0 interface, a 1 GB LPDDR4 RAM, and a slot for a microSD card. The microSD card is not included in the scope of delivery and must be ordered separately, taking the desired memory capacity into account.

CX8280 | Embedded PC with Arm® Cortex®-A53 and RS232/RS485
The CX8280 Embedded PC has two serial interfaces, one with RS232 and one with RS485 physics. These are both located on the D-sub socket. They are not bound to any particular protocol and can be used with the corresponding TwinCAT 3 Functions for the different serial communication protocols.

CX8290 | Embedded PC with Arm® Cortex®-A53 and 2-port Ethernet switch
The CX8290 Embedded PC is a controller with a second, switched Ethernet port. Protocols such as real-time Ethernet, ADS UDP/TCP, and EAP (EtherCAT Automation Protocol) are supported, and additional real-time protocols such as PROFINET, EtherNet/IP™, and BACnet/IP can be retrofitted via TwinCAT Functions.