Mar 6, 2024

Powerful, precise, and dynamic: XTS as an extended gantry system

Beckhoff's XTS is a highly flexible and efficient transport system that is used in a variety of applications, specifically automation technology. The XTS consists of a modular track system and magnetically driven movers that enable precise positioning and fast transportation of objects.As the movers can be positioned as desired and can be controlled independently of each other, the XTS is perfect for complex assembly and handling tasks. If heavy loads need to be moved, then two XTS systems can be linked together, creating a compact parallel system that allows the weight to be distributed evenly across several movers.