OdpniPripniZapri

Dec 6, 2023

Smooth workflows with TwinCAT 3, MATLAB®, Simulink® and Stateflow

TwinCAT enables MathWorks products to be integrated very flexibly. You can create a position controller in Simulink® to control a real axis or train AI for a visual quality inspection in MATLAB® and execute it in the controller: all this and more can be achieved with TwinCAT Targets for MathWorks products.

More about this video

MATLAB® and Simulink® for TwinCAT 3

MATLAB® and Simulink® for TwinCAT 3

With the current TwinCAT 3 target products, it is possible to transfer analyses and simulations from MATLAB® and Simulink® directly into the TwinCAT world.

TE1400 | TwinCAT 3 Target for Simulink®

TE1400 | TwinCAT 3 Target for Simulink®

TwinCAT 3 Target for Simulink® provides an interface between Simulink® and TwinCAT. The Simulink® software is developed and distributed by the MathWorks company. The programming environment is based on MATLAB® and is widely used both in science and in industry. Simulink® is a graphic programming environment that is ideally suited to the model-based development process. Simulation models of systems can be created and, for example, control and feedback control algorithms in order to test the models created.

TE1401 | TwinCAT 3 Target for MATLAB®

TE1401 | TwinCAT 3 Target for MATLAB®

TwinCAT 3 Target for MATLAB® provides an interface between MATLAB® and TwinCAT. MATLAB®, the language of technical computing, is developed and distributed by the MathWorks company. The programming environment is widely used both in science and in industry. MATLAB® is a script language that is ideally suited for the development of algorithms and mathematical models.

TE1410 | TwinCAT 3 Interface for MATLAB® and Simulink®

TE1410 | TwinCAT 3 Interface for MATLAB® and Simulink®

MATLAB® and Simulink® are developed and distributed by the MathWorks company. The two programming environments are widely used both in science and in industry. Simulink® is a graphic programming environment that is ideally suited to the model-based development process. MATLAB® is a script language for the development of algorithms and mathematical models.