AtsietiPataisytiUždaryti

Biuras Kaune
Beckhoff Automation OÛ

Karaliaus Mindaugo ave. 38
44307 Kaune, Lietuva

+370 605 42400
info@beckhoff.lt
www.beckhoff.com/lt-lt/

Dec 1, 2022

High-quality stainless steel control panels with an IP65 protection rating

The CP39xx-14xx control panel series with a stainless steel finish are control and operating devices that meet stricter hygiene requirements, especially designed for the pharmaceutical, food, and packaging industries. In this video, we demonstrate the special features of these control panels with IP65 protection.

More about this video

CP39xx-1400-0010 | Stainless steel multi-touch Control Panel with CP-Link 4 – The One Cable Display Link

CP39xx-1400-0010 | Stainless steel multi-touch Control Panel with CP-Link 4 – The One Cable Display Link

The Control Panels from the CP39xx-14xx series in a stainless steel finish are control and operating devices that meet strict hygiene requirements – above all important in the pharmaceutical, food and packaging industries. The Control Panels with IP65 protection are characterized by an optimized housing design with minimized gaps.

CP39xx-1401-0010 | Stainless steel multi-touch Control Panel with CP-Link 4 – The One Cable Display Link

CP39xx-1401-0010 | Stainless steel multi-touch Control Panel with CP-Link 4 – The One Cable Display Link

The Control Panels from the CP39xx-14xx series in a stainless steel finish are control and operating devices that meet strict hygiene requirements – above all important in the pharmaceutical, food and packaging industries. The Control Panels with IP65 protection are characterized by an optimized housing design with minimized gaps.

CP39xx-1414-0010 | Stainless steel multi-touch Control Panel with CP-Link 4 – The One Cable Display Link

CP39xx-1414-0010 | Stainless steel multi-touch Control Panel with CP-Link 4 – The One Cable Display Link

The Control Panels from the CP39xx-14xx series in a stainless steel finish are control and operating devices that meet strict hygiene requirements – above all important in the pharmaceutical, food and packaging industries. The Control Panels with IP65 protection are characterized by an optimized housing design with minimized gaps.

Packaging machines

Packaging machines

PC-based control significantly increases the productivity and flexibility of packaging machines and lowers the consumption of resources.