PC-based control technology from Beckhoff is exceptionally scalable in terms of hardware and software, enabling precisely tailored solutions for every application. As an answer for cost-sensitive applications in the lower and medium performance range, two new entry-level Beckhoff Industrial PCs (IPCs) have been announced to achieve best-in-class results at a lower price-point. The new additions are the C6905 Control Cabinet PC and the CP6706 Panel PC, which feature Intel® Atom™ multi-core CPUs with options for one, two or four processor cores.
More about this video
![PCs](/media/pictures/tiles/products/ipc/ipc.png)
PCs
With self-developed and produced motherboards, the Beckhoff Industrial PCs combine performance with flexibility, stability, and long-term availability.
![Panel PCs](/media/pictures/tiles/products/ipc/panel-pc.png)
Panel PCs
The Beckhoff Panel PCs, in the versions as built-in devices or mounting arm devices in IP65, combine modern touch technologies with flexible computing power.
![Control Panels](/media/pictures/tiles/products/ipc/control-panel.png)
Control Panels
As the front end of a machine, the Beckhoff Control Panels are its visual and functional business card and allow a wide range of customer-specific adaptations.
![C65xx | Fanless built-in Industrial PCs](/media/pictures/tiles/products/ipc/c6515-control-cabinet-ipc.png)
C65xx | Fanless built-in Industrial PCs
The C65xx series of fanless Industrial PCs is conceived for installation in the panel of the control cabinet or in the rear panel of a control or console housing.
![C6905 | Economy control cabinet Industrial PC](https://multimedia.beckhoff.com/media/c6905__web_main_preview.png)
C6905 | Economy control cabinet Industrial PC
The C69xx Industrial PC series is characterized by its compact design, the robust aluminum housings, and an especially wide choice of components and interfaces.
![CP6600, CP6606 | Economy built-in Panel PC](https://multimedia.beckhoff.com/media/cp6600__web_main_preview.png)
CP6600, CP6606 | Economy built-in Panel PC
The CP6600 and CP6606 built-in Panel PCs are designed for installation in the front of a control cabinet or control housing and can be used for a variety of applications in machine construction and plant engineering – for example, as a stand-alone controller with the TwinCAT automation software running on Windows Embedded Compact 7 or as a remote desktop display. They are available with two different touch screen displays with a 7 or 10.1-inch screen size.
![CP6700, CP6706 | Economy built-in Panel PC](https://multimedia.beckhoff.com/media/cp6700__web_main_preview.png)
CP6700, CP6706 | Economy built-in Panel PC
The CP6700 and CP6706 built-in Panel PCs are designed for installation in the front of a control cabinet or control housing and, with their highly integrated 3½-inch motherboard, they represent a powerful platform for use in machine construction and plant engineering, for example with the TwinCAT automation software running on Windows 10 IoT Enterprise. They are available with two different touch screen displays with a 7 or 10.1-inch screen size.