CX7000 | The small controller with integrated multi-function I/Os
Cost-effective and stand-alone compact controller with 480MHz processor and integrated multi-functional I/Os.
More about this video
![CX7000 | Embedded PC with Arm® Cortex®-M7 processor](https://multimedia.beckhoff.com/media/cx7000__web_preview.png)
CX7000 | Embedded PC with Arm® Cortex®-M7 processor
The CX7000 Embedded PC has an Arm® Cortex®-M7 single-core processor with 480 MHz. In the basic configuration, the CX7000 has a slot for a microSD card and an Ethernet interface. As a special feature, the CX7000 series has eight integrated multi-functional inputs as well as four integrated multi-functional outputs. The CX7000 does not have a fieldbus interface.
![CX7080 | Embedded PC for RS232/RS485](https://multimedia.beckhoff.com/media/cx7080__web_preview.png)
CX7080 | Embedded PC for RS232/RS485
The CX7080 Embedded PC has an Arm® Cortex®-M7 single-core processor with 480 MHz. In the basic configuration, the CX7080 has a slot for a microSD card and an Ethernet interface. As a special feature, the CX7000 series has eight integrated multi-functional inputs as well as four integrated multi-functional outputs. In addition, the CX7080 offers two serial interfaces, one with RS232 and one with RS485 physics. Both serial interfaces are on the D-sub socket.