הפרדהתיקוןסגירה
mx-system-einsatz-profilbearbeitungsmaschine-schirmer-stage-lowres

Feb 28, 2024

Automated profile processing with the MX-System, a modular automation solution

Our MX-System in action on the machine

We cordially invite you to visit Schirmer Maschinen GmbH's booth (Hall 3, Booth 217) at Fensterbau Frontale in Nuremberg from March 19 to 22. You can see our MX-System in its premiere in a PVC processing center, along with other innovations from the profile processing machinery specialist. We can demonstrate how this lean system solution is structured live in operation and show how both machine builders and end users can benefit from it.

Your Beckhoff sales contact can help you to register for a free visit to the exhibition.

The MX-System

The MX-System has taken automation to the next stage of evolution. All the tasks and properties of a classic control cabinet are packaged in a modular IP67-protected system that can be mounted on the machine. The time required to plan and build machines is reduced enormously for manufacturers, while end users benefit from a smaller footprint and optimized operation.