DetachFixClose

Apr 26, 2023

TwinCAT 3: Product news from Hannover Messe 2023

TwinCAT has been shaping the world of automation since 1996, with TwinCAT 3 already in its third generation. The latest developments in the TwinCAT automation suite, such as the features and properties of the new Build 4026 or the TwinCAT 3 Autotuning and the TwinCAT 3 Weighing Library products, are presented by our product experts in this video.

More about this video

TwinCAT 3 Build 4026

TwinCAT 3 Build 4026

More flexibility in automation development through modularity and extensions

TE5960 | TwinCAT 3 Autotuning

TE5960 | TwinCAT 3 Autotuning

Autotuning represents the simple commissioning and optimization of servo axes in machines. At the push of a button, the servo drive determines all essential parameters of the application within seconds.

TF3685 | TwinCAT 3 Weighing Library

TF3685 | TwinCAT 3 Weighing Library

The TwinCAT 3 Weighing PLC Library makes it possible to integrate a scale for weight measurement into the PC-based machine control system – particularly in conjunction with the I/Os of the ELM35xx and EL3356 EtherCAT Terminals. The focus is primarily on the dynamic weighing process. Signal filtering is particularly demanding here, as the weighing time has a significant influence on the overall processing time of the machine. Rapid signal filtering with the same level of precision produces a faster weight result, which ultimately makes for faster machines.