DetachFixClose

CX8200 Embedded PC series: higher computing power in a compact format

With the ARM Cortex™ A53 processor, the new CX82xx Embedded PC series from Beckhoff uses a modern CPU architecture with two cores, thus offering more computing power for compact controls.

More about this video

CX8200 | Embedded PC with Arm® Cortex®-A53 processor

CX8200 | Embedded PC with Arm® Cortex®-A53 processor

The CX8200 Embedded PC features an Arm® Cortex®-A53 dual-core processor running at 1.2 GHz. The basic configuration of the CX8200 includes a 1 Gbit Ethernet interface, a USB 3.0 interface, a 1 GB LPDDR4 RAM, and a slot for a microSD card. The microSD card is not included in the scope of delivery and must be ordered separately, taking the desired memory capacity into account. The CX8200 does not have a fieldbus interface.

CX8210 | Embedded PC with EtherCAT

CX8210 | Embedded PC with EtherCAT

The CX8210 Embedded PC is a control with an EtherCAT slave interface. It features an Arm® Cortex®-A53 dual-core processor with 1.2 GHz. The basic configuration of the CX8200 includes a 1 Gbit Ethernet interface, a USB 3.0 interface, a 1 GB LPDDR4 RAM, and a slot for a microSD card. The microSD card is not included in the scope of delivery and must be ordered separately, taking the desired memory capacity into account.

CX8280 | Embedded PC with RS232/RS485

CX8280 | Embedded PC with RS232/RS485

The CX8280 Embedded PC has two serial interfaces, one with RS232 and one with RS485 physics. These are both located on the D-sub socket. They are not bound to any particular protocol and can be used with the corresponding TwinCAT 3 Functions for the different serial communication protocols.

CX8290 | Embedded PC with different Ethernet protocols

CX8290 | Embedded PC with different Ethernet protocols

The CX8290 Embedded PC is a controller with a second, switched Ethernet port. Protocols such as real-time Ethernet, ADS UDP/TCP, and EAP (EtherCAT Automation Protocol) are supported, and additional real-time protocols such as PROFINET, EtherNet/IP, and BACnet/IP can be retrofitted via TwinCAT Functions.