AtsietiPataisytiUždaryti

Biuras Kaune
Beckhoff Automation OÛ

Karaliaus Mindaugo ave. 38
44307 Kaune, Lietuva

+370 605 42400
info@beckhoff.lt
www.beckhoff.com/lt-lt/

Oct 29, 2021

C69xx - The heart of PC-based control technology

The compact wonder for the control cabinet: The C69xx industrial PC series has a very compact design and a robust aluminum housing. Equipped with 3½-inch Beckhoff motherboards, the performance spectrum ranges from the very small, fanless C6915 with Intel® Atom™ CPU to the C6930 with processors up to Intel® Core™ i7 of the latest generation and on-board SATA RAID 1 controller.

More about this video

C69xx | Compact Industrial PCs

C69xx | Compact Industrial PCs

The C69xx Industrial PC series in a compact aluminum housing is characterized by the large selection and fine scalability of its components and interfaces.

C6905 | Economy control cabinet Industrial PC

C6905 | Economy control cabinet Industrial PC

The C69xx Industrial PC series is characterized by its compact design, the robust aluminum housings, and an especially wide choice of components and interfaces.

C6915 | Control cabinet Industrial PC

C6915 | Control cabinet Industrial PC

The C69xx Industrial PC series is characterized by its compact design, the robust aluminum housings, and an especially wide choice of components and interfaces.

C6920 | Control cabinet Industrial PC

C6920 | Control cabinet Industrial PC

The C69xx Industrial PC series is characterized by its compact design, the robust aluminum housings, and an especially wide choice of components and interfaces.

C6925 | Fanless control cabinet Industrial PC

C6925 | Fanless control cabinet Industrial PC

The C69xx Industrial PC series is characterized by its compact design, the robust aluminum housings, and an especially wide choice of components and interfaces.

C6930 | Control cabinet Industrial PC

C6930 | Control cabinet Industrial PC

The C69xx Industrial PC series is characterized by its compact design, the robust aluminum housings, and an especially wide choice of components and interfaces.

C6905-0010 | Economy control cabinet Industrial PC

C6905-0010 | Economy control cabinet Industrial PC

C6905-0020 | Economy control cabinet Industrial PC

C6905-0020 | Economy control cabinet Industrial PC

C6905-0030 | Economy control cabinet Industrial PC

C6905-0030 | Economy control cabinet Industrial PC

C6915-0010 | Fanless control cabinet Industrial PC

C6915-0010 | Fanless control cabinet Industrial PC

C6915-0020 | Fanless control cabinet Industrial PC

C6915-0020 | Fanless control cabinet Industrial PC

C6920-0060 | Control cabinet Industrial PC

C6920-0060 | Control cabinet Industrial PC

C6920-0070 | Control cabinet Industrial PC

C6920-0070 | Control cabinet Industrial PC

C6925-0030 | Fanless control cabinet Industrial PC

C6925-0030 | Fanless control cabinet Industrial PC

C6925-0040 | Fanless control cabinet Industrial PC

C6925-0040 | Fanless control cabinet Industrial PC

C6930-0060 | Control cabinet Industrial PC

C6930-0060 | Control cabinet Industrial PC

C6930-0070 | Control cabinet Industrial PC

C6930-0070 | Control cabinet Industrial PC