Aug 7, 2023

From the kitchen into the cloud – Digitalization recipe for the pancake of tomorrow

PC-based control facilitates data integration in food manufacturing

Yummy Bakery's pancakes are "hot" and end up on the shelves of virtually every major retail chain in Belgium. The secret behind this success? Using the authentic ingredients and preparation method on a baking plate. A recipe that perfectly combines with digitalization as CTRL Engineering successfully demonstrated. Besides 7 to 8% raw material savings, the automation of dough dosing with control technology from Beckhoff also helped provide data for ongoing process optimization.