In this Beckhoff Trade Show TV from EuroBLECH 2024, we will show where PC-based control from Beckhoff is used in sheet metal working, in particular on the machine from Baykal Machinery. We also show, how the MX-System can reduce the footprint of machines and systems.
More about this video

MX-System
Our MX-System combines all technological innovations in automation technology in an IP67-capable modular system.

Control Panels
As the front end of a machine, the Beckhoff Control Panels are its visual and functional business card and allow a wide range of customer-specific adaptations.

AX8000 | Multi-axis servo system
The AX8000 is the space-saving solution for applications with more than two axes. Extensive TwinSAFE functions allow a safe machine design.

AL8000 and AL8100 linear motors with One Cable Technology
Integrated OCT feedback system makes using linear motors exceptionally easy

Translatory servomotors
The direct drives are particularly suitable for applications with the highest requirements for dynamics, positioning accuracy and synchronism.

Sheet metal working
High performance built-in: PC-based control from Beckhoff for all control and drive applications in sheet metal working