Extrusion heads and extruders,for retrofitting blow molding machines
W. Müller GmbH, Germany
Servo-electric blow molding machine with 24" Control Panel from Beckhoff
Kautex Maschinenbau GmbH, Germany
横浜オフィス(本社)
ベッコフオートメーション株式会社
+81 50 1790 1111
info@beckhoff.co.jp
www.beckhoff.com/ja-jp/
W. Müller GmbH, Germany
Kautex Maschinenbau GmbH, Germany
Beckhoff has been a partner of leading companies in extrusion blow molding technology for many years. Hardware and software components from Beckhoff are used by a global customer base. From individual components to the complete solution, the user benefits from Beckhoff's broad process and application know-how in blow-molding technology. Beckhoff's extensive know-how in hydraulic drive technology, for example, leads to the best results with axes that are demanding in terms of control, such as transport movement, even with cost-reduced hydraulics. Modern servo-electric concepts are modularly integrated into the software architecture: machine programs for hydraulic, electric or mixed drive technology are created and maintained in an identical development environment. The core component of blow molding machines, parison control, is carried out with high precision in the entire range of different machine concepts.
The trend towards complete production cells is supported by the extensive Beckhoff hardware and software portfolio. As if from a construction kit, machine manufacturers can assemble a suitable control solution for their system or plant type. The automation toolkit comprises an extensive portfolio of Industrial PCs as well as control and display devices in all performance categories and form factors. EtherCAT, the global standard for real-time communication, offers maximum performance in integrating third-party power controllers. The Beckhoff I/O system covers a wide range of sensors and actuators and supports interfaces to different fieldbus systems. In TwinSAFE, Beckhoff has developed an integrated safety solution that reduces the engineering effort, especially for production cells, due to its flexibility. Servomotors and drives of all performance classes are available for the axis movement of electrically driven machines.
TwinCAT is the universal software platform for engineering, runtime and the diagnosis of all control functions: from PLC, motion control and robotics to HMI and vision, and from safety and measurement technology to cloud communication and the analysis functions. This ensures efficient interaction of all system components and enables maximum productivity. Special devices can be omitted due to the consistent implementation of all functionalities as software modules. This reduces not only hardware costs, but also engineering effort and lifecycle costs. In addition to extensive Motion Control software packages for electrical machines, TwinCAT also includes proven function blocks for hydraulic machines. These functions are supplemented by software libraries for the Euromap/OPC UA connection as well by the TwinCAT Plastic Application Components, into which Beckhoff's many years of experience in the plastics industry have been incorporated.
Beckhoff offers control components in software and hardware for extrusion blow molding machines with hydraulic or electric drive technology of all sizes, from simple single-head applications to complex multi-layer systems:
With the TwinCAT 3 Plastic Framework, we offer a modular software solution for the control of plastics machines that minimizes development effort and maintains the open nature of Beckhoff architecture. The TwinCAT 3 Plastic Framework brings together our many years of expertise in plastics, seamlessly integrating important industry-specific functions into the established TwinCAT environment. As a result, plastics machines can be programmed, visualized, and controlled on a single platform.
The TwinCAT 3 Plastic Framework contains three software libraries: TF8540 enables comprehensive software-based temperature control in plastics processing. TF8560 is a technology package that provides all the components for controlling motion functions in plastics machines. TF8550 is an HMI package specially developed for the plastics industry that enables the visualization of typical processes with minimal engineering effort and integrates seamlessly into the other technology packages.
Integrated, application-specific templates and sample code for various plastics applications facilitate project planning and programming, and are made available free of charge via the TwinCAT 3 Plastic Application. Of course, existing templates can also be used and your own process expertise can be integrated.
TF8540: Plastic Processing Framework
TF8560: Plastic Technology Functions
TF8550: Plastic HMI Framework
In TwinCAT HMI, the user has an innovative and sustainable tool at his disposal for creating user interfaces for blow molding machines. Prefabricated HMI components, such as the wall thickness editor, can be used directly or customized by the machine manufacturer. In addition to the display on the machine panel, the HTML5-based architecture also enables the presentation of machine data in the same design on mobile devices such as smartphones or touchpads. The HMI objects contain many functionalities, such as user administration with different access rights or a language changeover. The central operating side of the extrusion blow molding controller is the wall thickness curve. Through support for the multi-finger touch function, the blowing curve can be zoomed, analyzed and changed quickly and easily. Interpolation points and curve segments of the wall thickness curve can be represented in an easily recognizable way and defined flexibly by means of colored graduations.