AI-assisted engineering
with TwinCAT CoAgent

From chatbot to intelligent agent: TwinCAT Chat becomes TwinCAT CoAgent

Industrial automation is evolving rapidly, with new AI forms of technology acting as key drivers of innovation. Beckhoff recognized this technological progress early on and developed TwinCAT CoAgent, an AI-based engineering assistant that significantly accelerates and streamlines industrial development processes. The new name highlights its role as an active, intelligent partner that helps companies achieve their efficiency goals.

TwinCAT CoAgent – AI-based assistant simplifies the engineering process
TwinCAT CoAgent – AI-based assistant simplifies the engineering process
The TwinCAT CoAgent architecture with access to specialized AI agents enables targeted support to be provided for a wide variety of tasks.
The TwinCAT CoAgent architecture with access to specialized AI agents enables targeted support to be provided for a wide variety of tasks.

Why TwinCAT CoAgent?

TwinCAT CoAgent offers comprehensive, intelligent support. As a digital assistant, the technology combines state-of-the-art generative AI models with custom-developed AI agents to accelerate development processes in PLC programming, I/O configuration, HMI design, and knowledge management, helping users achieve better results faster and more efficiently.

Cutting-edge AI technology for more efficient automation

The technological foundation is built on the most advanced generative AI models, which Beckhoff has optimized and integrated to meet the specific requirements of industrial automation. Thanks to their exceptional ability to quickly and accurately process natural language, images, and complex technical relationships, these AI models deliver high-quality solutions that significantly accelerate engineering processes.

The AI agents independently suggest concrete actions and actively assist engineers in developing control systems. In doing so, they specifically access the Beckhoff Information System to incorporate industry- and product-specific knowledge into the solutions they propose. TwinCAT CoAgent offers flexible and adaptive support – always guided by the experts in charge.

Putting people at the heart of automation

TwinCAT CoAgent was developed to effectively support and simplify the demanding work of engineers and developers. Final decisions and control over the AI-generated output always remain with the specialists involved, who can review, confirm, and approve all results for execution. The AI technology handles routine tasks, suggests efficient solutions, and frees up time for more complex activities. Responsibility remains with the people behind the process, supported every step of the way by intelligent assistance.

Outpacing the competition with speed and efficiency

AI technology delivers sustainable benefits through shorter development cycles, higher quality results, and increased productivity, creating clear competitive advantages. One of the ways TwinCAT CoAgent puts this into practice is by suggesting and generating automated unit tests for PLC code. This significantly improves software quality and helps identify errors early in the development process.

The AI agents of TwinCAT CoAgent

TwinCAT CoAgent includes specialized agents, each with its own logic, designed to support and optimize different areas of automation.

Creating PLC code becomes faster and more intuitive. Requirements can be conveniently described in natural language, after which TwinCAT CoAgent suggests suitable Structured Text code. Libraries and existing project structures are automatically taken into account, ensuring that all suggestions are relevant and context-specific. Integrated code search functions and simple referencing of libraries further simplify development and help improve code quality.

Configuring I/O topologies and communication interfaces is now easier than ever. Hardware modules can be created, named, and configured via chat. The AI provides targeted suggestions for I/O configuration, helping reduce errors and accelerate commissioning. Users retain full control over decisions and fine-tuning at all times, ensuring both flexibility and customization.

With TwinCAT CoAgent, it couldn’t be easier to create modern user interfaces. The AI assistant uses simple sketches to automatically generate complete HMI pages, identify controls, flexibly adapt design themes, and suggest appropriate code for server extensions. Automatically linking PLC variables reduces the time required during the creation process. Whether you’re building comprehensive layouts or making quick adjustments, every step can be conveniently controlled via chat. The AI handles all the groundwork, leaving the user in full control to verify results and make individual adjustments as needed.

TwinCAT CoAgent has direct access to documentation in the Beckhoff Information System, enabling the AI to search it as needed. This allows users to receive tailored suggestions and recommendations aligned with their current requirements and project context. As a result, information retrieval is streamlined, making everyday tasks much easier.

Products

TE1700 | TwinCAT 3 CoAgent New

TE1700 | TwinCAT 3 CoAgent

TwinCAT 3 CoAgent is the intelligent AI assistant that provides efficient support for PLC development, I/O configuration, and human-machine interface creation. Requirements can be formulated in normal language and TwinCAT CoAgent suggests suitable code and configurations, taking existing project structures into account. Flexible mode selection enables custom support based on the task at hand. In addition, TwinCAT CoAgent offers direct access to the documentation in the Beckhoff Information System and provides context-related recommendations for accelerated high-quality project implementation.

TE1000 | TwinCAT 3 Engineering

TE1000 | TwinCAT 3 Engineering

TE1000 is the TwinCAT development environment for convenient configuration of control, drive control and I/Os. In addition, the tool includes the configuration and programming of TwinSAFE, the safety solution from Beckhoff.