![Process automation for the energy sector PC-based control is the universal control platform for process technology applications. © Beckhoff](/media/pictures/stages/branches/prozessindustrie/process_industry_stage_energy_industry_1160x520.jpg)
Integrates process technology into the overall control system:
Process automation for the energy sector
![Energy management with Beckhoff](/media/pictures/stages/campaign_energy_stage.jpg)
Representative office Egypt
Integrates process technology into the overall control system:
Optimizing energy and process efficiency using forward-thinking control solutions is one of the key criteria for the sustainable development of urban environments. Efficient solutions based on intelligent networking are required in all relevant areas - from sustainable energy generation in decentralized biogas plants and intelligent energy-saving systems to control of district heating systems and smart cities.
In the case of biogas systems, the control requirements appear to be less complex at first glance. However, in order to ensure the economic efficiency of a plant and maximize energy yield, the microbiological process requires optimum conditions such as temperature, pH value and pressure to be continuously monitored by the control system. Faults or events that exceed the maximum values must be identified automatically and reported to the operator. What is also important for most decentralized plants is the possibility to implement remote monitoring and control. The requirements are even more complex when it comes to automating intelligent storage systems, which are used to compensate for frequency fluctuations when supplying sustainable energy sources. These systems store energy in case of excess capacity, so that they can feed back into the grid if production bottlenecks arise. This requires optimum energy storage management based on continuous recording and monitoring of energy data and fast communication using telecontrol protocols. Forward-thinking solutions for efficient energy generation therefore require the highest degree of connectivity.
To meet these challenges, Beckhoff control technology supports all common communication standards in the area of fieldbus systems and the software-based integration of all common communication protocols. Reliability, fast data transmission, flexibility and powerful scalability to implement cost-effective solutions are important requirements in the energy sector. These requirements can be ideally met with PC-based automation. A comprehensive portfolio of measurement technology modules enables reliable recording of temperature, pressure and flow rates, for example. Condition monitoring and power monitoring can also be integrated into the automation platform via corresponding interfaces to provide a basis for predictive maintenance and the evaluation of raw current and voltage data.