TwinCAT HMI

Simple to use. Your fastest way to the solution. Platform-independent: TwinCAT HMI.

What does the HMI solution of the future look like? How can the all-important user interface be given an industry-spanning design in the future so that maximum operator efficiency and optimum user comfort are ensured? Today, Beckhoff is pioneering the way to the next generation of HMI solutions with TwinCAT HMI: TwinCAT now integrates the Human Machine Interface directly into the familiar environment of Microsoft Visual Studio®. Programming is unnecessary as configuration is handled with ease using the TwinCAT HMI graphical editor. As simple as the configuration is, the handling is equally adaptable: this web-based solution, which is based on HTML5 Simple to use. Your fastest way to the solution. Platform-independent: TwinCAT HMI. We reserve the right to make technical changes. BECKHOFF New Automation Technology 3 and JavaScript, acts “responsively”, irrespective of the operating system, browser and device. The powerful basic architecture makes numerous application scenarios possible: from the local panel dis lay solution to multi-client, multi-server and multi-runtime concepts. Individual extensions can be implemented quickly via defined interfaces; the mix of standard controls and custom design elements facilitates individualisation and differentiation.
 

Products

TE2000

TE2000: The TC3 HMI (human-machine interface) integrates itself into the well-known Visual Studio® development environment.

TF2000

TF2000: The TC3 HMI Server is a modular web server that provides the human-machine interface (HMI).

Further Information