Download Video: MP4, WebM, Ogg

Beckhoff is presenting the CX2000 series – the second generation of its Embedded PC family which was brought onto the market in 2002. The CX2030 and CX2040 Embedded PCs implement an essential new feature: multi-core processors. With this impressive boost in performance, these embedded controllers cover performance areas previously reserved for larger, cabinet-mounted Industrial PCs. A further essential feature of the new Embedded PC series is the internal extension bus, which is based on PCI Express and with which the system interfaces are connected with the full bandwidth of a PCI Express lane.



CX2020: The fanless Embedded PC has a 1.4 GHz Intel® Celeron® CPU.


CX2030: The CX2030 is also fanless and has a 1.5 GHz Intel® Core™ i7 dual-core CPU.


CX2040: Due to its high power the CPU of the CX2040 (2.1 GHz Intel® Core™ i7 quad-core) is equipped with a fan with ball bearings and speed monitoring.