Download Video: MP4, WebM, Ogg

C5210 | 19-inch slide-in Industrial PC with only one height unit

With the new C5210 Industrial PC, Beckhoff is extending its series of 19-inch slide-in Industrial PCs with a device with only one height unit and thus satisfies the growing demand for control devices with a flat design. The C5210 has an Intel® Celeron® processor 1.9 GHz, 2 cores, on a 3½-inch motherboard and is equipped with an on-board RAID controller and two SATA 3½-inch hard drive removable frames. The Industrial PC can be extended with PCIe modules, a Mini PCI card or a DVD drive.